S08QE8 with External Oscillator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S08QE8 with External Oscillator

1,080 次查看
MatthewScott_DE
Contributor II

I am designing with the 16 pin S08QE8 and plan to use an external oscillator (not a crystal or resonator).  Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging or is there another setup that should be used?

 

Thank you very much for your time

标签 (1)
0 项奖励
回复
4 回复数

942 次查看
MatthewScott_DE
Contributor II

Thank you both very much

0 项奖励
回复

942 次查看
rocco
Senior Contributor II

Hi Matthew Scott,

 

Welcome to the forum.


Do I drive the EXTAL pin with the oscillator output and leave the XTAL pin hanging?

Yes.

 

0 项奖励
回复

942 次查看
bigmac
Specialist III

Hello,

 

An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.

 

Regards,

Mac

 

0 项奖励
回复

942 次查看
rocco
Senior Contributor II

bigmac wrote:

An additional consideration may be, that if ICSC2_EREFS bit is set to zero, the XTAL pin should be available as GPIO.


Good point. You do not need to "leave it hanging". You can do something useful with it.

0 项奖励
回复