S08JS series USB bootloader protocol

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S08JS series USB bootloader protocol

ソリューションへジャンプ
2,558件の閲覧回数
gravis
Contributor I

I develop on and use Linux exclusively so I'm looking for Linux substitute for the BOOTLOADER_GUI (under "Snippets, Boot Code, Headers, Monitors, etc.") that I can use.  Since I'm convinced none exists, I'm interested in the protocol used and information that I can use to write a driver (if needed).  I know there is BDM but I was hoping to avoid that so I can provide firmware updates if needbe.

 

Thanks.

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 解決策
2,364件の閲覧回数
pgo
Senior Contributor V

Hi Gravis,

USBDM provides a GUI bootloader (Linux/Win) for loading the USBDM software into a JS16 using the Freescale bootloader protocol.

It might be a good starting point.

The AN3958 application note describes the Bootloader  protocol (search for AN3958 on the Freescale site).

bye

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,365件の閲覧回数
pgo
Senior Contributor V

Hi Gravis,

USBDM provides a GUI bootloader (Linux/Win) for loading the USBDM software into a JS16 using the Freescale bootloader protocol.

It might be a good starting point.

The AN3958 application note describes the Bootloader  protocol (search for AN3958 on the Freescale site).

bye

0 件の賞賛
返信
2,364件の閲覧回数
gravis
Contributor I

the AN3958 pdf was what i was really looking for though it's super low level but i'll take it. :smileyhappy:

0 件の賞賛
返信