S08JS series USB bootloader protocol

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08JS series USB bootloader protocol

Jump to solution
2,328 Views
gravis
Contributor I

I develop on and use Linux exclusively so I'm looking for Linux substitute for the BOOTLOADER_GUI (under "Snippets, Boot Code, Headers, Monitors, etc.") that I can use.  Since I'm convinced none exists, I'm interested in the protocol used and information that I can use to write a driver (if needed).  I know there is BDM but I was hoping to avoid that so I can provide firmware updates if needbe.

 

Thanks.

Labels (1)
Tags (5)
0 Kudos
Reply
1 Solution
2,134 Views
pgo
Senior Contributor V

Hi Gravis,

USBDM provides a GUI bootloader (Linux/Win) for loading the USBDM software into a JS16 using the Freescale bootloader protocol.

It might be a good starting point.

The AN3958 application note describes the Bootloader  protocol (search for AN3958 on the Freescale site).

bye

View solution in original post

0 Kudos
Reply
2 Replies
2,135 Views
pgo
Senior Contributor V

Hi Gravis,

USBDM provides a GUI bootloader (Linux/Win) for loading the USBDM software into a JS16 using the Freescale bootloader protocol.

It might be a good starting point.

The AN3958 application note describes the Bootloader  protocol (search for AN3958 on the Freescale site).

bye

0 Kudos
Reply
2,134 Views
gravis
Contributor I

the AN3958 pdf was what i was really looking for though it's super low level but i'll take it. :smileyhappy:

0 Kudos
Reply