S08JM60 USB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08JM60 USB

6,772 Views
alexismercier
Contributor III

Hi all,

I'm a newbie in USB and I've to program the JM60 as a USB mass storage.

I've already used the Freescale USB Stack v4.1.1 and the JM60 is'nt recognized by windows ( XP) .

If somebody can help me he's welcome.

regards

Alexis MERCIER

Labels (1)
0 Kudos
Reply
12 Replies

6,457 Views
alexismercier
Contributor III

I also tried to install with the .inf file but no results.

thanks for help

Alexis MERCIER

0 Kudos
Reply

6,457 Views
weapon
Senior Contributor I

I also test the board in windows XP, works fine, even needn't to install driver.

Did you try to reconnect the USB plug ? I mean plug out then plug in again.

In addition, you can try to make the board work standalone (without debugger),

Move th jumper cap in J3 to MiniUSB_VDD, then plug the USB to PC, the board will be powerd on by PC USB.

0 Kudos
Reply

6,457 Views
alexismercier
Contributor III

Hi,

I don't work on a DemoJM Board so I Have'nt any jumper  .

I tried to reconnect the USB plug and there is no result again.

0 Kudos
Reply

6,457 Views
weapon
Senior Contributor I

If so, it's possible that the issue is caused by the board.  could you show me the schematic of your board?

0 Kudos
Reply

6,457 Views
alexismercier
Contributor III

Can you give me your e-mail to send you  the schematic please.

0 Kudos
Reply

6,457 Views
weapon
Senior Contributor I
0 Kudos
Reply

6,457 Views
alexismercier
Contributor III

I'll try to get it in the afternoon

Regards

0 Kudos
Reply

6,457 Views
alexismercier
Contributor III

screenshot1.bmp

0 Kudos
Reply

6,457 Views
alexismercier
Contributor III

Hi Weiping,

thanks a lot for your help. The program compile but my 60 stays as an unknown device and windows tell me that it's work normally

0 Kudos
Reply

6,457 Views
weapon
Senior Contributor I

Hi,

Please use CW10.x project, the path is like:C:\Freescale\Freescale USB Stack v4.1.1\Source\Device\app\msd\cw10\s08usbjm60.

It can work in DemoJM60 board.  There is compile error in CW classic project, sorry.

B.R

XWP

6,457 Views
alexismercier
Contributor III

Hi weiping,

thaks for your answer.

I haven't CW10 so it will be a little complicated.

Best Regards

Alexis MERCIER

0 Kudos
Reply

6,457 Views
weapon
Senior Contributor I

Hi Alexis,

ok, if you want to use CW classic, please modify the compiler option as below,  after doing that the project can work.

1. Select standard setting

option.jpg

2. Modify the compiler option

Modify.jpg

3. After download the program to DemoJM60, we can see the device in hardware manager.

HardwareMgr.jpg