S08, how to disable pins to decrease power comsuption?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S08, how to disable pins to decrease power comsuption?

Jump to solution
2,550 Views
w_tension
Contributor III


The DOCs suggest "Configure port pins to minimize current drain", But didn't mention HOW-TO.

Labels (1)
Tags (1)
1 Solution
2,296 Views
kef2
Senior Contributor V

Current drain rises when digital input floats between '0' and '1' levels. To eliminate it do one of the following on all your unused digital inputs:

1) turn input to output using data direction registers

2) enable pull device, both pull-up and pull-down are OK.

3) pull inputs externally to I/O supply rails, usually vss or vdd

Since lower pin count packages may have non bonded out pin pads, you should not forget to turn them into outputs as well.

Edward

View solution in original post

4 Replies
2,297 Views
kef2
Senior Contributor V

Current drain rises when digital input floats between '0' and '1' levels. To eliminate it do one of the following on all your unused digital inputs:

1) turn input to output using data direction registers

2) enable pull device, both pull-up and pull-down are OK.

3) pull inputs externally to I/O supply rails, usually vss or vdd

Since lower pin count packages may have non bonded out pin pads, you should not forget to turn them into outputs as well.

Edward

2,296 Views
w_tension
Contributor III

Thanks, I'm using MC9S08QG4 TSSOP-16.

As I see in its datasheet, Max pin number is 24, So I should take them in count too.

0 Kudos
Reply
2,296 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

Also remember disable all the modules that you are not using

I do not know the family that you are using but please check the following application note

AN4441

2,296 Views
w_tension
Contributor III

Thanks, I've read the document.

0 Kudos
Reply