RS08 sensor temperature

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RS08 sensor temperature

1,353 次查看
christopheferna
Contributor I

Hi everyone,

 

I have been trying to get the temperature from the value of the temperature sensor channel of the MC9RS08KB2 microcontroller.

The problem that i have is that i can not find the "VTEMP25" and "m" values for calculate the temperature.

Someone can tell me where I can find these values?

 

Regards.

标签 (1)
0 项奖励
回复
1 回复

1,163 次查看
arpitaagarwal-b
NXP Employee
NXP Employee

Hello,

One of our TIC engineer has given these values, though I don't have the weblink for the same.

Temp Sensor Slope:

−40°C– 25°C               1.646  mV/°C

25°C– 125°C                1.769 mV/°C

Temp Sensor Voltage:

VTEMP25   =  701.2 mV

This might help.

If this post helps you, kindly mark it as correct/helpful answer.

-Arpita

0 项奖励
回复