RE: HC908QT4 Internal osc.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RE: HC908QT4 Internal osc.

3,395 Views
wf_lee
Contributor I
I'm using HC908QT4 and internal osc. I've set the OSCOPT1:0 to 00 in CONFIG2 but the OSC2 on PTA4 (OSC2EN=1) shown it's only ~3.9MHz not 12.8MHz as stated in the datasheet.
 
Any suggestion what goes wrong? Thx!
 
Labels (1)
0 Kudos
Reply
1 Reply

1,163 Views
joerg
Contributor II
Hi wf.lee
Since the bus clock is one fourth of f osc -> this is correct! The internal osc runs at 12.8MHz (nominal, +/-25%) so maximum bus clock frequency will bee 4MHz (means f osz = 16MHz). For a adjusted osz. frquency you have to programm the OSCTRIM register with the right value.

Saluti joerg
0 Kudos
Reply