RE: HC908QT4 Internal osc.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RE: HC908QT4 Internal osc.

3,396件の閲覧回数
wf_lee
Contributor I
I'm using HC908QT4 and internal osc. I've set the OSCOPT1:0 to 00 in CONFIG2 but the OSC2 on PTA4 (OSC2EN=1) shown it's only ~3.9MHz not 12.8MHz as stated in the datasheet.
 
Any suggestion what goes wrong? Thx!
 
ラベル(1)
0 件の賞賛
返信
1 返信

1,164件の閲覧回数
joerg
Contributor II
Hi wf.lee
Since the bus clock is one fourth of f osc -> this is correct! The internal osc runs at 12.8MHz (nominal, +/-25%) so maximum bus clock frequency will bee 4MHz (means f osz = 16MHz). For a adjusted osz. frquency you have to programm the OSCTRIM register with the right value.

Saluti joerg
0 件の賞賛
返信