QG8-FREQUENCY CHANGE TO...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QG8-FREQUENCY CHANGE TO...

3,431 Views
HarrySun
Contributor I
Hello,
 
in debuging mode with QG8,the window located at the right corner of debugger always shows "Frequency change to ~0","Frequency change to ~55296","Frequency change to ~998656h",these three messages shows alternatively many times(the set frequency is 1mhz).
I understand this means the debugger is trying to synchronize QG8, but why is it changing all the time?does this mean QG8 frequency is changing all the time too?
 
thanks  very much


Message Edited by HarrySun on 2008-02-05 03:21 PM
Labels (1)
0 Kudos
Reply
4 Replies

2,361 Views
JimDon
Senior Contributor III
In a word, yes that is what it means.
I have seen this when using an external  xtal, I put a scope probe on the xtal, causing to oscillate erratically.

What are you using for clocks?

0 Kudos
Reply

2,361 Views
HarrySun
Contributor I
thanks Jim.
 
I use the 16-MHz internal clock and bus frequency is set to 1Mhz.
but why is it changing all the time?
when it is "0",does that  mean the inteneral clock stops?
 
thanks a lot
0 Kudos
Reply

2,361 Views
JimDon
Senior Contributor III
It means the BDM thinks thats it's 0.
You settings sound perfectly ok. Did you use PE to generate the init code?
What BDM are you using? - I will try it tonight and see....
0 Kudos
Reply

2,361 Views
HarrySun
Contributor I
Jim,
 
thanks very much for your prompt reply.
I didn't use PE ,I coded the initial setting myself.
I use P&E USB multilink,HCS08/HCS12 and coldeworrior IDE version is 5.7.0
 
 
0 Kudos
Reply