QE32 Dual Serial " Back to Back" Mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QE32 Dual Serial " Back to Back" Mode

757 Views
Designer11
Contributor IV

Hi Everyone,

 

I am working on a project that required the use of the dual SCI because of the differences in baud rate. The target device baud rate is fixed at 230K and the PC/Controller to the MCU  is running anywhere from 9600 to 115K baud.

 

Below is  the configuration:

 

|PC/Other Devices|<--------------SCI1----------->|MCU|<-------SCI2----------->|Target Device|

 

My question is does anyone have sample codes or known of any application notes that discussed about this kind of configuration and would it be possible to have the two serials work in this mode ?

 

Thanks in Advance,

 

D

Labels (1)
0 Kudos
Reply
1 Reply

599 Views
bigmac
Specialist III

Hello,

 

Any data received by SCI1 (at the lower baud rate) may be immediately written to SCI2D register, from within the SCI1 receive ISR.  SCI2 should always be ready to handle the new transmit data.

 

The potential problem will be the sending, via SCI1, of the data received by SCI2 - data can arrive at a faster rate than it can be re-sent.  You will obviously need a FIFO (circular) buffer that is written by the SCI2 receive ISR, and is also accessed by the SCI1 transmit ISR.  It would be up to the SCI2 receive ISR to ensure that SCI1 transmit (TDRE) interrupt became enabled wnen any new data was received.

 

What happens next will depend on the nature of the received data - whether the buffer can be made large enough to hold each data burst, and whether there is sufficient time between data bursts to re-send the data at the lowest baud rate.

 

If not, you will need to prevent butter overflow by the implementation of handshaking for SCI2.  This handshaking may be of the "hardware" type, using CTS or DSR signals.  Alternatively, "software" (Xon/Xoff) handshaking may be feasible.  Whatever method you use, it will need to match that implemented within the target device.

 

Regards,

Mac

 

0 Kudos
Reply