Programming with Command Line

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Programming with Command Line

2,633 Views
edasanli
Contributor I

I have a MC9S08PA4 microprocessor. I need programming with command line. Does anybody have a solution about this? I prefer Linux but i can use Windows too if i have to. 

Thank you,

Eda SANLI

0 Kudos
Reply
3 Replies

2,623 Views
vicentegomez
NXP TechSupport
NXP TechSupport

You can use the command line on codewarrior 11.x for that.

Regards

 

0 Kudos
Reply

2,614 Views
edasanli
Contributor I

If you have, can you please share some examples about that? I used CodeWarrior Flash Programming from a DOS shell. I created a tcl file and I used it with -vmargsplus command. But i need to do flash programming witout opening CodeWarrior IDE.

With my best regards.

0 Kudos
Reply

2,604 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry I only do it with codewarrior.

 

0 Kudos
Reply