Programming with Command Line

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming with Command Line

2,659件の閲覧回数
edasanli
Contributor I

I have a MC9S08PA4 microprocessor. I need programming with command line. Does anybody have a solution about this? I prefer Linux but i can use Windows too if i have to. 

Thank you,

Eda SANLI

0 件の賞賛
返信
3 返答(返信)

2,649件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

You can use the command line on codewarrior 11.x for that.

Regards

 

0 件の賞賛
返信

2,640件の閲覧回数
edasanli
Contributor I

If you have, can you please share some examples about that? I used CodeWarrior Flash Programming from a DOS shell. I created a tcl file and I used it with -vmargsplus command. But i need to do flash programming witout opening CodeWarrior IDE.

With my best regards.

0 件の賞賛
返信

2,630件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Sorry I only do it with codewarrior.

 

0 件の賞賛
返信