Programming MC9RS08KA8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming MC9RS08KA8

4,210件の閲覧回数
Florijan
Contributor III
Hi,

I am going to use RS08KA8 uC in future projects and I can see that you need 12V on RESET pin in order to program or erase flash. Can anybody please tell me, can P&E HCS08 USB Multilink generate this 12V voltage on RESET pin or do I have to provide this voltage some other way?

Best regards,
Florijan
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,376件の閲覧回数
Florijan
Contributor III
Hi,

Good news. Today I received samples of RS08KA8 and I was able to programm it using P&E Multilink Rev. C without any problems, just like S08 devices.

Regards,
Florijan
0 件の賞賛
返信

2,376件の閲覧回数
JimDon
Senior Contributor III
USB-ML-12-
HCS08, HC(S)12(X), RS08, and ColdFire V1 microcontrollers

However, for HC08 you will need USB-ML-MON08.

0 件の賞賛
返信

2,376件の閲覧回数
Florijan
Contributor III
Hi,

Thank you both for responses. Probably I will order semples of KA8 and try it then I will post results in this forum.

best regards,
Florijan
0 件の賞賛
返信

2,376件の閲覧回数
LightElf
Contributor I
I never worked with RS08, BUT:
my P&E USB Multilink marked with "Rev. C" and "For  RS08 - HCS08 - HC(S)12(X)" on the bottom mark.
0 件の賞賛
返信

2,376件の閲覧回数
bigmac
Specialist III
Hello Florijan,
 
The high programming voltage was also required for the older HC908 series.  If the latest offering of the USB Multilink is still capable of programming these devices, it should be capable of supplying the high voltage for the RS08 devices.  Perhaps check the P&E website.
 
Regards,
Mac
 
0 件の賞賛
返信