Program Multiple Target Boards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program Multiple Target Boards

2,039件の閲覧回数
Designer11
Contributor IV

Hello Everyone,

 

We are in the production phase and would like to know would it be possible to use either the (one) Cyclone Pro, or USB multilink to program multiple target boards.  Or does anyone know of any other products in the market  that offer this capability ?

We are using the HCS08 series.

 

 

 

Thanks,

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,587件の閲覧回数
Juls
Contributor III

we use cyclone pro

but its 1 unit programmed by cyclone

but you can get more cyclone

as a standalone its pretty easy  you dont need a pc conected to program each unit

only a properly configured cyclone

0 件の賞賛
返信

1,587件の閲覧回数
Designer11
Contributor IV

Yes, i am using the cyclone pro too. I tried to connect two boards in parralel to the cyclone but it didn't  work/program.

0 件の賞賛
返信

1,587件の閲覧回数
bigmac
Specialist III

Hello,

 

You cannot parallel two boards!  It is one board at a time connected to a Cyclone, because the BKGD/MS pin utilises data transfer in both directions.

 

The previous comment made referred to the possibility for the Cyclone to operate stand alone, without the need to always be connected to a computer.  This would simplify the use of multiple Cyclone Pros, but still only with a single board connected to each one at any instant.

 

Regards,

Mac

 

 

 

0 件の賞賛
返信