TSS: Xtrinsic Touch Sensing Software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TSS: Xtrinsic Touch Sensing Software

1,821 Views
roberto_m
Contributor III

Hi to all,

 

is there anyone that alrey use TSS? What is your opinion?

Is it possible to wake up the micro with a touch key?

Labels (1)
0 Kudos
Reply
2 Replies

1,361 Views
DanielMtz
NXP Employee
NXP Employee

Well this will depends, of which library you are using, and which operation mode you configure, for stop 2 is not possible, for wait and stop 3 if you configure KBI measurement method, available in TSS 2.0, probably you could wake up the MCU, other way to make this is waking up the MCU with a timer interrupt and call the TTS Task function to check the electrode status.       

0 Kudos
Reply

1,361 Views
roberto_m
Contributor III

really, no one experienced this software ?:smiley surprised:

0 Kudos
Reply