Program Flash - when to reset watchdog

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program Flash - when to reset watchdog

Jump to solution
9,029 Views
Bjerring
Contributor I

Hi all

 

I'm in the process of changing one of our older products and in that process I'm planning to enable the watchdog. My problem is that I get a watchdog timeout when my program erase/write the flash

 

the erase and write routines looks like they are directly take from the HCS08 Family Reference Manual and looks like the following


 

FlashErase1:psha             lda     #(mFPVIOL+mFACCERR) ;mask            sta     FSTAT               ;abort any command and clear errors            lda     #mPageErase         ;$40 mask pattern for page erase command            bsr     DoOnStack           ;finish command from ram-based sub            ais     #1            rts                         ;Z = 0 means there was an error;*********************************************************************DoOnStack:  pshx            pshh                        ;save pointer to flash            psha                        ;save command on stack            ldhx    #SpSubEnd           ;point at last byte to move to stackSpMoveLoop: lda     ,x                  ;read from flash            psha                        ;move onto stack            aix     #-1                 ;next byte to move            cphx    #SpSub-1            ;past end?            bne     SpMoveLoop          ;loop till whole sub on stack            tsx                         ;tsx=stack på indexreg.point to sub on stack            tpa                         ;move CCR to A for testing            and     #$08                ;check the I mask            bne     I_set               ;skip if I already set            sei                         ;block interrupts while FLASH busy            lda     SpSubSize+6,sp      ;preload data for command            jsr     ,x                  ;execute the sub on the stack            cli                         ;ok to clear I mask now            bra     I_cont              ;continue to stack de-allocationI_set:      lda     SpSubSize+6,sp      ;preload data for command            jsr     ,x                  ;execute the sub on the stackI_cont:     ais     #low(SpSubSize+3)   ;deallocate sub body + H:X + command                                        ;H:X flash pointer OK from SpSub            lsla                        ;A=00 & Z=1 unless PVIOL or ACCERR            rts                         ;to flash where DoOnStack was called ;*********************************************************************SpSub:      ldhx    low(SpSubSize+4),sp      ;get flash address from stack            sta     0,x                 ;write to flash; latch addr and data            lda     SpSubSize+3,sp      ;get flash command            sta     FCMD                ;write the flash command            lda     #mFCBEF             ;mask to initiate command            sta     FSTAT               ;[pwpp] register command            nop                         ;[p] want min 4~ from w cycle to rChkDone:    lda     FSTAT               ;[prpp] so FCCF is valid            lsla                        ;FCCF now in MSB            bpl     ChkDone             ;loop if FCCF = 0SpSubEnd:   rts          SpSubSize   equ     *- (SpSub)            ;back into DoOnStack in flash ;*********************************************************************FlashProg1: psha                        ;temporarily save entry data            lda     #(mFPVIOL+mFACCERR) ;mask            sta     FSTAT               ;abort any command and clear errors            lda     #mByteProg          ;mask pattern for byte prog command            bsr     DoOnStack           ;execute prog code from stack RAM            ais     #1                  ;deallocate data location from stack            rts                         ;Z = 0 means there was an error;*********************************************************************

 

 


so my problem is where do I "feed the dog"  in this routine so it dont timeout (it need to be feed every 23ms) I guess it needs to be in the subroutine that run in the RAM but I can't really figure out where

 

hope someone of you can help

 

best regards

Mikkel

Labels (1)
0 Kudos
Reply
1 Solution
8,059 Views
kef
Specialist I

SpSub:      ldhx    low(SpSubSize+4),sp      ;get flash address from stack
            sta     0,x                 ;write to flash; latch addr and data
            lda     SpSubSize+3,sp      ;get flash command
            sta     FCMD                ;write the flash command
            lda     #mFCBEF             ;mask to initiate command
            sta     FSTAT               ;[pwpp] register command
            nop                         ;[p] want min 4~ from w cycle to r
ChkDone:    lda     FSTAT               ;[prpp] so FCCF is valid
            lsla                        ;FCCF now in MSB
            <<<<<<<<<<<<<<<<<<<<<<<< feed the dog here

            bpl     ChkDone             ;loop if FCCF = 0
SpSubEnd:   rts

View solution in original post

0 Kudos
Reply
17 Replies
8,060 Views
kef
Specialist I

SpSub:      ldhx    low(SpSubSize+4),sp      ;get flash address from stack
            sta     0,x                 ;write to flash; latch addr and data
            lda     SpSubSize+3,sp      ;get flash command
            sta     FCMD                ;write the flash command
            lda     #mFCBEF             ;mask to initiate command
            sta     FSTAT               ;[pwpp] register command
            nop                         ;[p] want min 4~ from w cycle to r
ChkDone:    lda     FSTAT               ;[prpp] so FCCF is valid
            lsla                        ;FCCF now in MSB
            <<<<<<<<<<<<<<<<<<<<<<<< feed the dog here

            bpl     ChkDone             ;loop if FCCF = 0
SpSubEnd:   rts

0 Kudos
Reply
8,059 Views
Bjerring
Contributor I

Thanks Kef

 

Short and precisely what I needed :smileyhappy:

 

again thanks for you time

 

Best regards

Mikkel

 

0 Kudos
Reply
8,059 Views
Brax02
Contributor III

So if you do that like this if there is a probleme with the erase (FCCF never come to '1'). The programm is blocked here.

 

For software who need a high level of security it's not good.

 

Somebody has a solution to solve this problem ?

0 Kudos
Reply
8,059 Views
bigmac
Specialist III

Hello, and welcome to the forum.

 

It is possible that the COP timer reset process may affect the MCU flags, particularly the Z and N flags. A more suitable position for this code would be immediately following the ChkDone: label. You can then also remove the NOP padding instruction just prior to the label.

 

As Kef suggests, it is also wise to test the FSTAT register for either of the error flags set, in addtion to the FCCF flag, and exit the loop should any of these flags become set.  In fact this seems to be required by the device datasheet / reference manual.  The test can be done with a single AND #$70 instruction in lieu of the LSLA. Looping would exit when the result becomes non-zero.

 

I also notice that the issue of globally disabling interrupts has not been covered by the code.  The interrupt vectors also become inaccessible during flash erase and programming.  This should be done within the code that calls the 'DoOnStack' routine.

 

I have used the following RAM based C function to do a similar thing, in a slightly different context.  This is the only code that needs to be RAM resident.

 

void flash_cmd( void)
{
   FSTAT = 0x80;                  // Clear FCBEF bit - activate command

   do {
      __RESET_WATCHDOG();
   } while ((FSTAT & 0x70) == 0); // Wait for command completion or error
}


 

Regards,
Mac

 

0 Kudos
Reply
8,059 Views
kef
Specialist I

Mac,

 

ACCERR and PVIOL in every decent implementation of flash routines are checked before issuing flash command and executing above mentioned doonstack routine. Even if you ignore it, FCCF will stay set.

 

  • So if you do that like this if there is a probleme with the erase (FCCF never come to '1'). The programm is blocked here.

I took this as something happens like controller gets damaged or doesn't resist nice EMI burst, so that FCCF never comes to 1. If this happens, then checking error bits in a loop most likely won't help. Defensive programming requires timeout for every wait for something loop, especially when this something is external event. I think COP should be reset only in the main application loop or in the lowest prioroty task. Long routine / process, one may have, doesn't justify resetting COP in 2nd place.

0 Kudos
Reply
8,059 Views
bigmac
Specialist III

Hello Kef,

 

The issue that I see is that the ACCERR or PVIOL flag may become set during the execution of the flash command, under circumstances where the FCCF bit may not become set.  Hence the additional exit conditions for the loop.  I seem to recall that this aspect is addressed in the datasheet flow diagrams.

 

The other issue is that the sector erase period may exceed the COP timeout period, and I assumed that this was the reason for the original query.  Clearing the COP timer from outside the loop won't help when this is the case.

 

Regards,

Mac

 

0 Kudos
Reply
8,059 Views
kef
Specialist I

Mac,

 

No, FCCF indicates where flash command is being executed or not. FCCF always is set after command completes, or if command was ignored due to errors.

 

I looked into S08D, S08GB, and S12C datasheets. All flash diagrams are looping checking only FCCF flag.

 

Yes, 20ms erase time can be longer than you want for COP timeout. I meant that resetting COP in flash routine is as bad as waiting until FCCF becomes set. 

0 Kudos
Reply
8,059 Views
bigmac
Specialist III

Hello Kef,


kef wrote:

 

I looked into S08D, S08GB, and S12C datasheets. All flash diagrams are looping checking only FCCF flag.

 


The flowcharts for the S08 (Fig. 4.2) actually show a separate 'error exit' from the loop, in addition to the normal exit when FCCF becomes set.

 

I do not know whether you are correct about FCCF also becoming set after an error occurs, but to conform with the datasheet, the error flags should also be tested within the loop.  Of course there is no reason why all three flags should not be simultaneously tested, and the error state then separately determined after exit from the loop has occurred.

A minor point - the page erase period may actually extend to about 26 milliseconds at the lower limit of the flash clock frequency (4000 cycles at 150kHz).

 

Regards,

Mac

 

0 Kudos
Reply
8,059 Views
kef
Specialist I

I don't know what derivative you are talking about, but all diagrams I saw clearly show only one loop, which is only waiting for FCCF=1. Loop is not entered if eroors occur after or before launching the flash command.

0 Kudos
Reply
8,059 Views
bigmac
Specialist III

Hello Kef,

 

I checked the datasheets for the 'QG8, 'SE8 and 'GB60.  Fig. 4.2 appears similar for all of them, and is a flow chart showing the erase and programming sequences.  Following the launching of the flash command, I see a single wait loop with two exits - an error exit and a normal exit.

 

Regards,

Mac

 

0 Kudos
Reply
8,059 Views
kef
Specialist I

See attached flow chart from GB60 datasheet. I see wait for FCCF=1 loop only. Yellow. Errors are checked once, no loop.

0 Kudos
Reply
8,059 Views
bigmac
Specialist III

Hello Kef,

 

Agreed that the testing of the error flags, and the error exit, are not part of the wait loop.  But it appears these flags still need to be tested after the command is launched (delayed by a few cycles).  Actually, in the interests of code size minimisation, it should not  matter if the error flags were tested within the wait loop, as I was proposing.

 

The SpSub routine in the original code snippet did not provide the error flag test afer the command was launched.

 

Regards,

Mac

 

0 Kudos
Reply
8,059 Views
bigmac
Specialist III

Hello,

 

Subsequent to my previous post, I found that a few devices do not specify the requirement for an error flag check immediately after starting the flash command.  After reviewing the Reference manual for quite a few different devices, I found the following exceptions.

 

AC128, AC60 (but not AC16):

Error check not required for byte programming and sector erase, but still required for burst programming.

DN/DV/DZ series, EL32/SL16:

Error check not required for sector erase, but required for byte or burst programming.

MM128, QE128 only, JE128, and SC4:

No error check required.

 

All other devices examined specifically required the error check for sector erase, byte program and burst program operations.

 

I cannot see that there would be any disadvantage in checking the error flags, either prior to or within the wait loop, even if not specifically required.  This would make the code more derivative independent.

 

Interestingly, many of the devices not specifically requiring the error flag test, also have paged flash memory and a MMU module.  These must necessarily be coded differently anyway, to make use of the LAP registers, in order to be able to program any flash byte.

 

Regards,

Mac

 

0 Kudos
Reply
8,059 Views
Brax02
Contributor III

 

  

 

Hello,

 

Thanks for your answer.

 

Someting like that could be a solution ?

 

                      LDHX #$FFFF      ;load count value to reset WD

ChkDone:    lda     FSTAT         ;[prpp] so FCCF is valid
                      lsla                        ;FCCF now in MSB
                

                      AIX    #-1
                      CPHX   #0
                      BEQ    NoEraseWD   ;if 0 no reset WD
              
                       LDA     #85          ;for have any Watchdog during erease
                       STA     SRS          ;Clear WatchDog counter - first part
                       LDA     #170
                       STA     SRS          ;Clear WatchDog counter - second part

NoEraseWD:  

                        bpl     ChkDone             ;loop if FCCF = 0

SpSubEnd:   rts

 

0 Kudos
Reply
8,058 Views
bigmac
Specialist III

Hello,

 

I can see two problems with your proposed code -

 

  1. The looping back to ChkDone is determined by the state of the N bit within the CPU status register.  However, the N bit state will be affected by the CPHX, LDA and STA instructions that are present prior to the loop.  This will not give the intended operation.
  2. The H:X value can continue decrementing from $0000 back to $FFFF, and so on.  Again this will not give the intended operation of maintaining the bypass of the COP timer clearing process.

The following code is intended to correct these deficiencies.  While COP processing occurs, the total loop period will be 29 cycles.  This means that COP processing will cease after approximately 1900000 cycles (i.e. 190 milliseconds for 10MHz bus frequency).  This compares with a sector erase period of about 25 milliseconds

 

...     LDHX  #$FFFFChkDone:     CPHX  #0     BEQ   SkipWD     AIX   #-1          ; Clear COP timer     LDA   #$55     STA   SRS     LDA   #$AA     STA   SRSSkipWD:     LDA   FSTAT     AND   #$70     ; Test for command complete or error     BEQ   ChkDone    ; Loop if not     RTS

 

Regards,

Mac

 

 

0 Kudos
Reply
8,057 Views
Brax02
Contributor III

You are right. My code was wrong.

 

For the time of the loop I will change the count value of 0xFFFF to a small one to have a watchdog reset after more than 35ms.

 

Thanks a lot for you help !

 

 

 

 

0 Kudos
Reply
8,057 Views
kef
Specialist I

That's another story. Yes, if flash controller hangs, your code will hang there too. To handle flash controller failure, you need to provide your own timeout mechanism, like for every other condition, which you are waiting for and which may never occur.

0 Kudos
Reply