Problems downloading program using PE loader for s08aw32

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problems downloading program using PE loader for s08aw32

1,615 次查看
chinniwhites
Contributor II

I was using a mc9s08aw16cfue but then recently had to change to mc9s08aw32cfue to get more memory/flash.  Using PE s08 loader tool, I select the correct s8p file for the s08aw32, but it fails to load program to micro.  The s8p file I was using for the s08aw16 is hc9s08aw16a while the file for the s08aw32 is s08aw32.  Any clues to what I am doing wrong here?

标签 (1)
0 项奖励
回复
1 回复

1,409 次查看
weapon
Senior Contributor I

Hi Chinniwhites,

Which tools you are using? P&E Multilink or Cyclone Pro?

In addition, just remind, MC9S08AW16A is different part with MC9S08AW16, 16A is enhanced verison, some periphrals in AW16A are newer version than AW16.

0 项奖励
回复