Problem with a MC68HC908AP16

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with a MC68HC908AP16

2,261 次查看
JrCL
Contributor I
Good day, I have a problem with a MC68HC908AP16, when I work him at 3v it doesn't begin, the pin RTS stays in under, if I work him at 5v it works well that I can make so that it works me at 3v. 
 
Thank you
标签 (1)
0 项奖励
回复
2 回复数

1,460 次查看
bigmac
Specialist III
Hello, and welcome to the forum.
 
The 908AP16 is unsuitable for operation from 3.3 volts.  The Vdd voltage range specified in the datasheet is 4.5-5.5 volts.
 
As the supply voltage increases, the LVI module will remain in the reset condition until the Vdd rises above typically 3.45 volts (3.65 volts maximum threshold).  But the normal operating voltage should not be less than 4.5 volts.
 
Regards,
Mac
 
0 项奖励
回复

1,460 次查看
Klined
Contributor I
The 908AP16 functional operating range is specified as being 2.7-5.5V in its datasheet.  The 908AP16A is specified to run @ 4.5-5.5V.

K

0 项奖励
回复