Problem with a MC68HC908AP16

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with a MC68HC908AP16

2,370件の閲覧回数
JrCL
Contributor I
Good day, I have a problem with a MC68HC908AP16, when I work him at 3v it doesn't begin, the pin RTS stays in under, if I work him at 5v it works well that I can make so that it works me at 3v. 
 
Thank you
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,569件の閲覧回数
bigmac
Specialist III
Hello, and welcome to the forum.
 
The 908AP16 is unsuitable for operation from 3.3 volts.  The Vdd voltage range specified in the datasheet is 4.5-5.5 volts.
 
As the supply voltage increases, the LVI module will remain in the reset condition until the Vdd rises above typically 3.45 volts (3.65 volts maximum threshold).  But the normal operating voltage should not be less than 4.5 volts.
 
Regards,
Mac
 
0 件の賞賛
返信

1,569件の閲覧回数
Klined
Contributor I
The 908AP16 functional operating range is specified as being 2.7-5.5V in its datasheet.  The 908AP16A is specified to run @ 4.5-5.5V.

K

0 件の賞賛
返信