Problem with CW10.5 debugger and PA4 VTG cpu with flash security option ON

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem with CW10.5 debugger and PA4 VTG cpu with flash security option ON

622 次查看
gpadam
Contributor I

Even a simple led blinking project seems to show the problem. If I set the NV_FSEC_INIT @0x0000FF7FU = 0x7DU the application would not start after bdm removing and issueing a cpu reset. During flash programming a " device is secure. Erase to unsecure" message appear but then tha application would not start at all. It seems the flash is secured prior to dco trimming and flash updating......

标签 (1)
0 项奖励
回复
0 回复数