Problem with CW10.5 debugger and PA4 VTG cpu with flash security option ON

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem with CW10.5 debugger and PA4 VTG cpu with flash security option ON

853件の閲覧回数
gpadam
Contributor I

Even a simple led blinking project seems to show the problem. If I set the NV_FSEC_INIT @0x0000FF7FU = 0x7DU the application would not start after bdm removing and issueing a cpu reset. During flash programming a " device is secure. Erase to unsecure" message appear but then tha application would not start at all. It seems the flash is secured prior to dco trimming and flash updating......

ラベル(1)
0 件の賞賛
返信
0 返答(返信)