Problem to send 13 bit LIN Break!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem to send 13 bit LIN Break!

1,188件の閲覧回数
mehdializadeh
Contributor II

Hi
I use mc9s08dz96. I wrote the corresponding registers to create a break at the beginning of the data LIN frame. The data frame is sent correctly, but the problem is that the break part is not 13 bits. I set the break registers like this:

 

  if (SCI1S1_TDRE == 0U) {            
    return ERR_TXFULL;              
  }
  SCI1C2_SBK = 0x01U;                
  SCI1C2_SBK = 0x00U;                

 

Then I send 0x55 and ID:

 

while(1){
  if (SCI1S1_TDRE == 0U) {       
    return ERR_TXFULL;            
  }
  SCI1C2_SBK = 0x01U;             
  SCI1C2_SBK = 0x00U;                 

  delayy(10);
  c=AS1_SendChar(Sync_);
  delayy(10);
  c=AS1_SendChar(ID_);
  delayy(333);
	}

 

I initialized these registers:

 

void AS1_Init(void)
{
  SerFlag = 0x00U;                     /* Reset flags */
  /* SCI1C1: LOOPS=1,SCISWAI=0,Rsrc=1,M=0,WAKE=1,ILT=0,PE=0,PT=0 */
  setReg8(SCI1C1, 0xA8U);              /* Configure the SCI */ 
  /* SCI1C3: R8=0,T8=0,TXDIR=1,TXINV=0,ORIE=0,NEIE=0,FEIE=0,PEIE=0 */
  setReg8(SCI1C3, 0x20U);              /* Disable error interrupts */ 
  /* SCI1C2: TIE=0,TCIE=0,RIE=0,ILIE=0,TE=0,RE=0,RWU=0,SBK=0 */
  setReg8(SCI1C2, 0x00U);              /* Disable all interrupts */ 
  /* SCI1S2: LBKDIF=0,RXEDGIF=0,??=0,RXINV=0,RWUID=0,BRK13=1,LBKDE=0,RAF=0 */
    setReg8(SCI1S2, 0x04U);               
SCI1BDH = 0x00U;                     /* Set high divisor register (enable device) */
    SCI1BDL = 0x1AU;                     /* Set low divisor register (enable device) */
    SCI1C2_TE = 0x01U;                  /* Enable transmitter */
    SCI1C2_RE = 0x01U;}

 

 BRK13 defines for us that the break length is 13. If you have noticed in the registers above, I have set it.

 

setReg8(SCI1S2, 0x04U);

 

 Finally, the frame LIN is like this:

mehdializadeh_0-1672053275696.png

Break is correctly sent, also 0x55, 0x34 for sync and ID, respectively. But the break length is not 13 bits. what is the reason?

 

0 件の賞賛
返信
0 返答(返信)