Problem in Power-Up on MC9RS08KA2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Problem in Power-Up on MC9RS08KA2

1,730 次查看
rs8
Contributor I
Hi at All
I have chk one big problem in the production circuit when I have used the MC9RS08KA2 microprocessor.
In a 20% on  the Board the program not run correctly when the system is power-up. But in the board non function if I switch  more time switch-off switch-on the power the system start well.
The problem is in  the low rise time on power supply? or is the LVD problem?
There is any solution?

Franco

标签 (1)
0 项奖励
回复
1 回复

968 次查看
peg
Senior Contributor IV
Hello rs8,
I think will will need much more detail of your setup before any meaningful answers can be given.
What does "not run correctly" mean?
You may need to get your code to check the SRS register and output its code somehow if it becomes a unexpected value.
Have you properly bypassed the supply?
What voltage are you running on?
etc?

0 项奖励
回复