Please Need help with DS1307 C programming code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please Need help with DS1307 C programming code

5,312件の閲覧回数
kilopondio
Contributor I
Hi all!,
 
I just need help with some C programming code for a DS1307 device.THe micro that I`m using is the 68HC908GP32.
 
Please I`m not an expert in this stuff and I found out some routine but no one work out properly.
 
Would anybody have some code that works correctly?
 
 
THank you very much!.
 
Kilopondio
 
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,440件の閲覧回数
mke_et
Contributor IV
I've not done it in C, but I have implemented it in assembly on a Star12. 
 
If you have a 'conceptual' question about it, fire away, but as to specifics in C, forget it.
 
Mike
 
0 件の賞賛
返信

1,440件の閲覧回数
UK_CF_FAE
NXP Employee
NXP Employee
Hi Kilopondio,
 
I think the chances of anyone having code to share with the DS1307 on this forum is pretty small.
 
Why not post the code that you're having difficulty with, and the members on this list can help you get it running.
 
Good luck
 
Mark
0 件の賞賛
返信