JBxx and USB ICP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JBxx and USB ICP

5,248件の閲覧回数
peg
Senior Contributor IV
Hello,
 
The links to AN2398SW appear to be broken on this site. :smileysad:
Can it be fixed? Can I get it elsewhere?
 
Also apart from the brief mention in AN2399, is the blank part ICP mode of the JB16 documented somewhere? The JB16 manual only seems to be aware of serial mode. I find it a little difficult to believe that 1/2 Meg pulldowns on a USB would be noticed.
 
TIA
Peg
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,035件の閲覧回数
Alban
Senior Contributor II
Hey Peg,
 
I think it's not documented because wasn't really for everyone at the start.
Maybe a big customer asked or someon suggested and it became the standard !
 
If we had heard before, Daniel would have made the TBDML (Turbo BDM Light, cheap programmer for S12) programmed from USB and the PCB would have been even smaller...
 
Ah "communication"...
 
Thanks for pinpointing the broken link.
 
Cheers,
Alban.
0 件の賞賛
返信

2,035件の閲覧回数
rocco
Senior Contributor II
Hi, Peg:

In case you can't find it anywhere else, I put a copy here:

http://www.remotehead.com/PrivateFolders/AN2398SWsoftware.zip

I also have the AN2399 software, if you need that as well.

Sorry I can't help on the ICP, except to agree that 1/2 mOhm pull-downs are not very significant.
0 件の賞賛
返信

2,035件の閲覧回数
Fonsi
Contributor I
If you have not gotten a hold of AN2398SW please submit an SR and as to be assigned to R23757.
 
Best Regards,
0 件の賞賛
返信