Open input pins can avoid with on chip pullup enable. E.g. for MS9S08QG8 must set Register PTBPE on

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Open input pins can avoid with on chip pullup enable. E.g. for MS9S08QG8 must set Register PTBPE on

跳至解决方案
1,772 次查看
Mei
Contributor IV

Open input pins can avoid with on chip pullup enable. E.g. for MS9S08QG8 must set Register PTBPE on addess 0x1844.

But I can't see reaction of write: mov $ff, PTBPE. 
I don't see any change to address $ 1840 while debugging, nor do I see defined levels on the B ports.
Programs with MC68HC08QT implemented a measurable internal resistance to + (VDD) at Pullupenable.

Can You help?

With best regards
Gerd

0 项奖励
回复
1 解答
1,747 次查看
Mei
Contributor IV

Dear Vicente,

thank you for your replay.

Yes, you are right. PTBPE must set in 0x1844.

But that wasn't the real mistake. Now I've found my mistake:

In my question I wrote: "But I can't see reaction of write: mov $ff, PTBPE."

Command --"mov $FF, PTBPE" -- is not suitable for setting the PTBPE register in 16 Bit address 0x1844, (High Page Registers)

Operand must be an 8 bit address in Direct Page Registers in lower address area.

E.g. PTBDD can be set with mov # $ FF, PTBDD.

In the case of PTBPE, I should have written: lda # $ FF sta PTBPE. Above the # sign was also missing.

I apologize for these simple assembler programming problems.

With best regards

Gerd Meinert

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,761 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

Can you confirm, please?

 

Should be check address 0x1844 not 0x1840

There is a sample code in ASM on the codewarrior samples code, you can use them as reference, normally is on the following folder

 

C:\...\CW MCU v11.1\MCU\CodeWarrior_Examples\HC_Examples\mc9s08qg8_demo

 

Regards

Vicente

 

0 项奖励
回复
1,748 次查看
Mei
Contributor IV

Dear Vicente,

thank you for your replay.

Yes, you are right. PTBPE must set in 0x1844.

But that wasn't the real mistake. Now I've found my mistake:

In my question I wrote: "But I can't see reaction of write: mov $ff, PTBPE."

Command --"mov $FF, PTBPE" -- is not suitable for setting the PTBPE register in 16 Bit address 0x1844, (High Page Registers)

Operand must be an 8 bit address in Direct Page Registers in lower address area.

E.g. PTBDD can be set with mov # $ FF, PTBDD.

In the case of PTBPE, I should have written: lda # $ FF sta PTBPE. Above the # sign was also missing.

I apologize for these simple assembler programming problems.

With best regards

Gerd Meinert

 

0 项奖励
回复