Off-Grid Solar Power Inverter

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Off-Grid Solar Power Inverter

2,295件の閲覧回数
paulbao
Contributor I

Hi,

I plan to design an Off-Grid Solar Power Inverter. The power is about 1000W.

Does anyone has any hardware and software solution for this project?

Many Thanks!

 

Paul BAo

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,045件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Paul,

I would like to recommend the Inverter for the Solar Panel using an MC56F8023.

You can find more information at:

http://www.freescale.com/files/dsp/doc/ref_manual/DRM126.pdf

Hope this information will be useful for you.

Have a great day.

Best Regards, :smileyhappy:

David Diaz.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,045件の閲覧回数
alex_pan
Contributor I

Hi David,

Also I have 1000W DC/AC project. I want to use MC56F827xx and want to refer  Solar Panel using an MC56F8023. But i couldn't find the detail schematic.You can find "The entire hardware and software design is available on the Freescale web."  in page44 from DRM126.pdf file. But NO entire hardware can be find. Could you please give me some help on this? 

Please send E_mail to the address [email protected] If you have detail schematic

Thanks

0 件の賞賛
返信