Off-Grid Solar Power Inverter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Off-Grid Solar Power Inverter

2,271 Views
paulbao
Contributor I

Hi,

I plan to design an Off-Grid Solar Power Inverter. The power is about 1000W.

Does anyone has any hardware and software solution for this project?

Many Thanks!

 

Paul BAo

Labels (1)
0 Kudos
Reply
2 Replies

2,021 Views
david_diaz
NXP Employee
NXP Employee

Hello Paul,

I would like to recommend the Inverter for the Solar Panel using an MC56F8023.

You can find more information at:

http://www.freescale.com/files/dsp/doc/ref_manual/DRM126.pdf

Hope this information will be useful for you.

Have a great day.

Best Regards, :smileyhappy:

David Diaz.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,021 Views
alex_pan
Contributor I

Hi David,

Also I have 1000W DC/AC project. I want to use MC56F827xx and want to refer  Solar Panel using an MC56F8023. But i couldn't find the detail schematic.You can find "The entire hardware and software design is available on the Freescale web."  in page44 from DRM126.pdf file. But NO entire hardware can be find. Could you please give me some help on this? 

Please send E_mail to the address [email protected] If you have detail schematic

Thanks

0 Kudos
Reply