Off-Grid Solar Power Inverter

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Off-Grid Solar Power Inverter

2,274 次查看
paulbao
Contributor I

Hi,

I plan to design an Off-Grid Solar Power Inverter. The power is about 1000W.

Does anyone has any hardware and software solution for this project?

Many Thanks!

 

Paul BAo

标签 (1)
0 项奖励
回复
2 回复数

2,024 次查看
david_diaz
NXP Employee
NXP Employee

Hello Paul,

I would like to recommend the Inverter for the Solar Panel using an MC56F8023.

You can find more information at:

http://www.freescale.com/files/dsp/doc/ref_manual/DRM126.pdf

Hope this information will be useful for you.

Have a great day.

Best Regards, :smileyhappy:

David Diaz.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,024 次查看
alex_pan
Contributor I

Hi David,

Also I have 1000W DC/AC project. I want to use MC56F827xx and want to refer  Solar Panel using an MC56F8023. But i couldn't find the detail schematic.You can find "The entire hardware and software design is available on the Freescale web."  in page44 from DRM126.pdf file. But NO entire hardware can be find. Could you please give me some help on this? 

Please send E_mail to the address [email protected] If you have detail schematic

Thanks

0 项奖励
回复