New baud rate ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

New baud rate ?

4,873 Views
CCandido
Contributor V

hcs08,

how to put new baud rate?

 

running 115200

 

int_sci1( 115200 );

run.....

now new baud rate ?

 

 

my code: init and close

void init_sci1( byte cfg,byte bh,byte bl ){     
   if( cfg ){
       
   SCI1C1= 0x00;             init
   SCI1C3= 0x00;
   SCI1S2= 0x00;               
   SCI1C2= 0x00;
               
   SCI1BDH = bh; // 0x000D =115200                     
   SCI1BDL = bl;                
     
   SCI1C3 |= 0x0F;                    
   SCI1C2 |= ( SCI1C2_TE_MASK | SCI1C2_RE_MASK | SCI1C2_RIE_MASK);
  
   } else {
       close
    SCI1C3 &= ~0x0F;                 
    SCI1C2 &= ( (~ SCI1C2_RE_MASK) & (~SCI1C2_TE_MASK) & (~SCI1C2_TIE_MASK) & (~SCI1C2_RIE_MASK));
    SCI1BDH = bh;            
    SCI1BDL = bl;

    }
     (void)SCI1D;
}

 

thanks,

Carlos,


//-------------------------------------------------------------------------

Labels (1)
0 Kudos
Reply
10 Replies

3,781 Views
bigmac
Specialist III

Hello Carlos,

 

You appear to have a 24MHz bus frequency.  Therefore the new baud rate divisor value can be calculated by the expression 1500000 / baud.  The value of 1500000 is derived from 24000000 / 16.

 

However, if you have an arbitrary baud rate value, and are using integer division, you will firstly need to provide "rounding"  to obtain the closer divisor value.  For example, for a baud rate of 153600, the calculated value would be 9, but a divisor of 10 gives a the closer result.

 

You would also need to be aware of the maximum allowable baud rate error, and provide a check that the calculated divisor value provides a sufficiently accurate result.  Not all baud rates may be feasible, and the baud rate function may need to check the accuracy.

 

Assuming all required baud rates are a multiple of 100, it would be better to use the (baud / 100) value for the calculations.  If you do this, the calculations will be more efficient because the value will remain within the bounds of an int, rather than require the use of a long integer.

 

When you write the divisor value to SCI1BD register, there is no need to write individually to the high and low bytes of the register.  For the 115200 baud case, the following would be sufficient -

SCI1BD = 13;

 

Finally, keep in mind that with the use of the very high baud rates, such as 115200, the SCI receive ISR would potentially need to be serviced every 86 microseconds (or 2080 cycles).  This means that the total execution period of the SCI receive ISR, plus any other ISR that may havet commenced just prior to the SCI interrupt, must be considerably less than the byte transmission period, to avoid loss of data.

 

Regards,

Mac

 

0 Kudos
Reply

3,781 Views
CCandido
Contributor V

Thanks for the replies.


but I want to know how to put new baud rate?
being in 4800 to 115200 and change for example.
just updating the value SCI1BDH / L, not the end, does not change the baud rate!
the problem is that after starting at 115200 are not changing to new value!

problems is not put new value in sci runnig.

 

thanks,

Carlos,

0 Kudos
Reply

3,781 Views
peg
Senior Contributor IV

Hello Carlos,

 

It should just be a matter of writing a new value to the baudrate registers.

The only limitation is that you must write high byte first low byte last, but you seem to be doing this.

Have you only tried 115200 and 4800 baud?

Going to 4800 baud involves a value in the high byte ($0138). What if you try for 9600 ($009D) just to see what happens.

Which exact S08 device are you using?

0 Kudos
Reply

3,781 Views
CCandido
Contributor V

Hello Peg

 

the problems no is CALC value in BR.

problems is new value SCI no modifier.....

ex:

 BR = 0x000D   <----init sci run.....

new

BR = 0x009D   <---------new value run...

 

results is =  0x000D    <---- see

 

thanks,

Carlos,

0 Kudos
Reply

3,781 Views
peg
Senior Contributor IV

Hello Carlos,

 

Again, which device are you using?

 

0 Kudos
Reply

3,781 Views
CCandido
Contributor V

Hello Peg

Im use JM60

 

Regards

Carlos,

0 Kudos
Reply

3,781 Views
CCandido
Contributor V

Hi

I use MC9S08JM60

 

he does not respond to a new baud rate.

ex: 115200 for 4800

 

thanks,

Carlos,

0 Kudos
Reply

3,781 Views
peg
Senior Contributor IV

Hi Carlos,

 

I would recommend starting a Service Request at this stage.

 

0 Kudos
Reply

3,781 Views
CCandido
Contributor V

Thanks for the replies. but I want to know how to put new baud rate? being in 4800 to 115200 and change for example. just updating the value SCI1BDH / L, not the end, does not change the baud rate! the problem is that after starting at 115200 are not changing to new value!

0 Kudos
Reply

3,781 Views
peg
Senior Contributor IV

Hello,

 

What makes you think it is not as simple as writing a new value to the baudrate registers?

 

0 Kudos
Reply