Need help getting mscan to sync

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help getting mscan to sync

1,393件の閲覧回数
boast
Contributor I

We're using a DEMO9S08DZ60-ND. We followed the appnotes for the mscan on the hc12, and modified it a bit. But mscan keeps getting stuck on the while loop trying to sync. We tried different sample code found online, and still nothing. The pins are only outputting 0V too.

 

void CANInit(void) {CANCTL0_INITRQ = 1; // enter initilization modewhile(!CANCTL1_INITAK); //wait until initialization mode is readyCANCTL1_CANE = 1; //enable mscan moduleCANCTL1_LOOPB = 1; //enable loopback modeCANCTL1_LISTEN = 0; //disable listen mode//set time segment 2 tq clock cycles to 3 CANBTR1_TSEG21 = 1;//set time segment 1 tq clock cycles to 6CANBTR1_TSEG12 = 1;CANBTR1_TSEG10 = 1;//set time quante of Synchronization jump width to 3 CANBTR0_SJW1= 1;// set clk prescale value to 3CANBTR0_BRP1 = 1; //disable identifier masking with don't cares. all messages received trigger interruptsCANIDMR0 = 0xFF;CANIDMR1 = 0xFF;CANIDMR2 = 0xFF;CANIDMR3 = 0xFF;CANIDMR4 = 0xFF;CANIDMR5 = 0xFF;CANIDMR6 = 0xFF;CANIDMR7 = 0xFF;CANCTL0_INITRQ = 0; // exit initialization modewhile(CANCTL1_SLPAK==1 && CANCTL1_INITAK==1); //wait until initialization mode exit successfullywhile(CANCTL0_SYNCH==0); //wait until mscan syncs}

 

 

not sure where exactly we're going wrong.

ラベル(1)
0 件の賞賛
返信
1 返信

1,192件の閲覧回数
kef
Specialist I

MSCAN is synchronized to the bus, when it receives valid message, send from different node. This probably won't ever happen in loopback mode.

0 件の賞賛
返信