Need help,MC3PHAC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Need help,MC3PHAC

2,821 次查看
sunny
Contributor I
I made a A/C motor drive board with MC3PHAC. The motor's rating is 220V/750W. Now the question is, when the motor runs at high speed(3000rpm/50Hz), everything is ok, but when it runs at 500rpm or slower, both the igbts and the motor become very hot. I don't know why? Can someone help me? Thanks!
标签 (1)
0 项奖励
回复
2 回复数

1,437 次查看
nedemek
Contributor I
Can u send schematic? or attach here?
0 项奖励
回复

1,437 次查看
poornirohit
Contributor I

Hi,

please help me i got stucked in sending the commands to mc3phac.it is not responding anything.

please help me........

thanks,

Poornima

0 项奖励
回复