Need help,MC3PHAC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need help,MC3PHAC

2,864件の閲覧回数
sunny
Contributor I
I made a A/C motor drive board with MC3PHAC. The motor's rating is 220V/750W. Now the question is, when the motor runs at high speed(3000rpm/50Hz), everything is ok, but when it runs at 500rpm or slower, both the igbts and the motor become very hot. I don't know why? Can someone help me? Thanks!
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,480件の閲覧回数
nedemek
Contributor I
Can u send schematic? or attach here?
0 件の賞賛
返信

1,480件の閲覧回数
poornirohit
Fresh Out Contributor

Hi,

please help me i got stucked in sending the commands to mc3phac.it is not responding anything.

please help me........

thanks,

Poornima

0 件の賞賛
返信