Need Info about deep sleep mode - MC13192

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Need Info about deep sleep mode - MC13192

ソリューションへジャンプ
2,762件の閲覧回数
mou
Contributor III
Hi,
 
Can anyone help me out with the information that to put the MC13192 ( with Microcontroller MC9S08GB60) device to deep sleep what hardware blocks need to be put off forcefully?Only putting the radio to hibernate or doze mode will not put the device to deep sleep.What needs to be done to put the device to deep sleep?Please help me in this regard.
I urgently need this information.
 
Regards,
Mou
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2007-11-28 10:52 AM
ラベル(1)
0 件の賞賛
返信
1 解決策
1,907件の閲覧回数
Mads
Contributor V
Hi Mou,
 
Please download our Beekit that contains the SMAC, MAC and ZigBee protocols.
In all of them there is functionality for handling low power mode.
 
Click on the Beekit banner.
 
Br,
Mads

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,908件の閲覧回数
Mads
Contributor V
Hi Mou,
 
Please download our Beekit that contains the SMAC, MAC and ZigBee protocols.
In all of them there is functionality for handling low power mode.
 
Click on the Beekit banner.
 
Br,
Mads
0 件の賞賛
返信