Need Info about deep sleep mode - MC13192

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need Info about deep sleep mode - MC13192

Jump to solution
2,767 Views
mou
Contributor III
Hi,
 
Can anyone help me out with the information that to put the MC13192 ( with Microcontroller MC9S08GB60) device to deep sleep what hardware blocks need to be put off forcefully?Only putting the radio to hibernate or doze mode will not put the device to deep sleep.What needs to be done to put the device to deep sleep?Please help me in this regard.
I urgently need this information.
 
Regards,
Mou
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2007-11-28 10:52 AM
Labels (1)
0 Kudos
Reply
1 Solution
1,912 Views
Mads
Contributor V
Hi Mou,
 
Please download our Beekit that contains the SMAC, MAC and ZigBee protocols.
In all of them there is functionality for handling low power mode.
 
Click on the Beekit banner.
 
Br,
Mads

View solution in original post

0 Kudos
Reply
1 Reply
1,913 Views
Mads
Contributor V
Hi Mou,
 
Please download our Beekit that contains the SMAC, MAC and ZigBee protocols.
In all of them there is functionality for handling low power mode.
 
Click on the Beekit banner.
 
Br,
Mads
0 Kudos
Reply