Monitor for QYA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Monitor for QYA

4,087 次查看
mikel
Contributor I
I'd like to know, if it's possibile to load the monitor program, used in the DEMO_BOARD that mounts the 68HC908QT4, for the 68HC908QY4A.
 
Thanks
 
Miche
标签 (1)
0 项奖励
回复
3 回复数

1,855 次查看
mikel
Contributor I

Thanks to all, but till now I've not been able to solve the problem. In fact the monitor program used in the Demo Board for the 68HC908QT4 (described in the application note AN2305) has some jumps to the QT/QY's ROM monitor program that for the QYA's ROM monitor has no sense. For example the jump to : IGetPut: equ $2D6B has a sense for the QY's ROM monitor, but for the QYA these are unimplemented memory location.

So the questions are, how must be re-addressed the jumps to the QY's ROM monitor program used in the AN2305 so that it works for the QYA family that has a different ROM monitor ?

 

Thanks

miche

 

 

0 项奖励
回复

1,855 次查看
bigmac
Specialist III

Hello Miche,

The likely difference that would affect the monitor program is that, with the A-suffix part is the internal oscillator defaults to a 1 MHz bus frequency, compared to 3.2 MHz for the "classic" part.  So the initialisation process will differ, in order to switch to the 3.2 MHz bus frequency.

Regards,
Mac

 

0 项奖励
回复

1,855 次查看
peg
Senior Contributor IV

Yes!

The QY is just a QT with an extra i/o port.

1,2 and 4 is just amount of flash.

1 to 2,4 is just an extra ADC module

There where many reports of recieving parts with more flash than what the part no. said and even ADC's in 1's.

I have used a QY4 (because I had some) in a project that originally used a QT1. Just ignore the extra pins (set as outs)

Regards David

 

Woops!

Wrote this, then noticed the A at the end.

So I will scale back my answer to probably, refer to EB658 to confirm.

 

Message Edited by peg on 2006-07-21 08:03 AM

0 项奖励
回复