Modify BeeKit code?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Modify BeeKit code?

2,971 Views
GaryOlmstead
Senior Contributor I
I need to have a full ZIgBee stack (not SMAC), but I am thinking about hardware other than the MC1321x series.  Is it possible to modify the BeeKit stack to accomodate a different transceiver?
 
Gary Olmstead
Toucan Technology
Ventura CA
 
Labels (1)
0 Kudos
Reply
3 Replies

1,705 Views
addiyi
NXP Employee
NXP Employee
Hello Gary,

Using BeeKit and BeeStack codebase, you can select the type of transceiver:  MC1319x, MC1320x or MC1321x. This property is only used when the Target hardware is set to User defined target configuration from Platform menu.

Regards,
Adrian
0 Kudos
Reply

1,705 Views
peg
Senior Contributor IV
Hi Gary,

I believe the license precludes this (must be used with Freescale hardware).


0 Kudos
Reply

1,705 Views
GaryOlmstead
Senior Contributor I
I can't find the license agreement; but it is certainly not possible from the BeeKit.  Guess I'll have to go to Plan B.
 
Thanks for your help.
0 Kudos
Reply