Modify BeeKit code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Modify BeeKit code?

3,110件の閲覧回数
GaryOlmstead
Senior Contributor I
I need to have a full ZIgBee stack (not SMAC), but I am thinking about hardware other than the MC1321x series.  Is it possible to modify the BeeKit stack to accomodate a different transceiver?
 
Gary Olmstead
Toucan Technology
Ventura CA
 
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,844件の閲覧回数
addiyi
NXP Employee
NXP Employee
Hello Gary,

Using BeeKit and BeeStack codebase, you can select the type of transceiver:  MC1319x, MC1320x or MC1321x. This property is only used when the Target hardware is set to User defined target configuration from Platform menu.

Regards,
Adrian
0 件の賞賛
返信

1,844件の閲覧回数
peg
Senior Contributor IV
Hi Gary,

I believe the license precludes this (must be used with Freescale hardware).


0 件の賞賛
返信

1,844件の閲覧回数
GaryOlmstead
Senior Contributor I
I can't find the license agreement; but it is certainly not possible from the BeeKit.  Guess I'll have to go to Plan B.
 
Thanks for your help.
0 件の賞賛
返信