Minimum Amplitude of the External Clock Input

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Minimum Amplitude of the External Clock Input

1,191 次查看
jiunnyang
NXP Employee
NXP Employee

As we know the PB is 5V system MCU, and the SU is also high operating voltage(4.5~18v).

How minimum amplitude of the external clock input for the MC9S08PB8VTG and MC9S08SU8?

is there okay for 3.3v OSC?

I can not find these parameters in Datasheet.

Thanks!

标记 (2)
0 项奖励
回复
1 回复

1,120 次查看
xuan_wu
NXP Employee
NXP Employee

Hi Jiunn,

You can find these parameters in the table: DC characteristics in S08PB/S08SU datasheet.

pastedImage_1.png

As shown in the above table, the minimum amplitude of external clock input can be calculated by the marked formula.

1. The voltage: Vddx = 5V,  the minimum high voltage of the pin: 0.70 x 5v = 3.5V,   3.3V OSC is not OK.

2. The 3.3V OSC is ok only if Vddx <=4.7V.

Thanks 

0 项奖励
回复