MCU Pin Variants

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU Pin Variants

Jump to solution
2,084 Views
MWMinor
Contributor V

I'm trying to use processor expert to generate code for an MC9S08AW60 application, and one of the set up screens asks about pin variants.

 

For example, MC9S08AW60CFU - what are these and where can I find the one applicable to my demo board...?

 

Thanks in advance

Labels (1)
0 Kudos
Reply
1 Solution
1,909 Views
MWMinor
Contributor V
0 Kudos
Reply
2 Replies
1,909 Views
kef
Specialist I

Have a look in AW datasheet at:

Appendix B Ordering Information and Mechanical Drawings

 

CFU is C - commercial temperature range (40C-85C), FU is 64pin QFP package.

0 Kudos
Reply
1,910 Views
MWMinor
Contributor V

Thank you...

0 Kudos
Reply