MC9S08SH8:I can enter in Stop3 mode but not in Stop2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08SH8:I can enter in Stop3 mode but not in Stop2

ソリューションへジャンプ
1,410件の閲覧回数
diegocolombo
Contributor IV

Kind support and community users

 

i'm evaluating MC9S08SH8 power consumption and behaviours in Stop3 and Stop2 modes.

 

Stop3 mode looks running,when entered the current consumption of my circuit(uC plus some low power peripherals) drops from 9 mA to 45 uA.

This does not happens launching Stop2.The  current consumption remains in the mA range

I am using Processor Expert to select the mode,the bit PPDC is write once,and i verify that PPDC=1 before running the "STOP" instruction,The other bits are conformed to table 3-1 of the datasheet .

 

What else should i check?

 

Thanks

 

Diego

ラベル(1)
0 件の賞賛
返信
1 解決策
1,125件の閲覧回数
diegocolombo
Contributor IV

It is my fault,sorry

The RESET/IRQ pin was left accidentaly floating.

Measuring the voltage it is low,so the IRQ is asserted,and this wakes the uC immediately or avoid that it enters i STOP2

Resoldering the pullup resistor makes it work correctly

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,126件の閲覧回数
diegocolombo
Contributor IV

It is my fault,sorry

The RESET/IRQ pin was left accidentaly floating.

Measuring the voltage it is low,so the IRQ is asserted,and this wakes the uC immediately or avoid that it enters i STOP2

Resoldering the pullup resistor makes it work correctly

0 件の賞賛
返信
1,125件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Diego

I glad to hear that your problem is solved.

If you have more problem, just let me know

Regards

Vicente Gomez

0 件の賞賛
返信
1,125件の閲覧回数
diegocolombo
Contributor IV

Thanks very much,Vicente

Diego

0 件の賞賛
返信