MC9S08SH8:I can enter in Stop3 mode but not in Stop2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S08SH8:I can enter in Stop3 mode but not in Stop2

跳至解决方案
1,332 次查看
diegocolombo
Contributor IV

Kind support and community users

 

i'm evaluating MC9S08SH8 power consumption and behaviours in Stop3 and Stop2 modes.

 

Stop3 mode looks running,when entered the current consumption of my circuit(uC plus some low power peripherals) drops from 9 mA to 45 uA.

This does not happens launching Stop2.The  current consumption remains in the mA range

I am using Processor Expert to select the mode,the bit PPDC is write once,and i verify that PPDC=1 before running the "STOP" instruction,The other bits are conformed to table 3-1 of the datasheet .

 

What else should i check?

 

Thanks

 

Diego

标签 (1)
0 项奖励
回复
1 解答
1,047 次查看
diegocolombo
Contributor IV

It is my fault,sorry

The RESET/IRQ pin was left accidentaly floating.

Measuring the voltage it is low,so the IRQ is asserted,and this wakes the uC immediately or avoid that it enters i STOP2

Resoldering the pullup resistor makes it work correctly

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,048 次查看
diegocolombo
Contributor IV

It is my fault,sorry

The RESET/IRQ pin was left accidentaly floating.

Measuring the voltage it is low,so the IRQ is asserted,and this wakes the uC immediately or avoid that it enters i STOP2

Resoldering the pullup resistor makes it work correctly

0 项奖励
回复
1,047 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Diego

I glad to hear that your problem is solved.

If you have more problem, just let me know

Regards

Vicente Gomez

0 项奖励
回复
1,047 次查看
diegocolombo
Contributor IV

Thanks very much,Vicente

Diego

0 项奖励
回复