MC9S08SH obsolete info

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08SH obsolete info

ソリューションへジャンプ
2,535件の閲覧回数
anandhram1988
Contributor I

hi, anybody can inform please the direct replacement for MC9S08SH32 ?

 

i found below, MC9S08SG32 and MC9S08EL32

in this case i would like to know the main differences between 

MC9S08SH32 vs  MC9S08SG32  vs MC9S08EL32

Many thanks in advance

1 解決策
2,482件の閲覧回数
Pablo_Ramos
NXP Employee
NXP Employee

Hi @anandhram1988,

The differences between the S08SH, S08SG, and S08EL are as follows:

S08EL includes the SLIC peripheral, which supports LIN 2.0 and SAE J2602 protocols. It also features 16 interrupt pins and up to 512 bytes of EEPROM.

S08SH features the MTIM peripheral, has only 8 interrupt pins, and supports a ganged output option that allows a single write to change the state of multiple pins simultaneously.

S08SG is similar to the S08SH in terms of pinout, tools, and software compatibility. However, it offers a wider range of package options.

Best regards,
Pablo

元の投稿で解決策を見る

1 返信
2,483件の閲覧回数
Pablo_Ramos
NXP Employee
NXP Employee

Hi @anandhram1988,

The differences between the S08SH, S08SG, and S08EL are as follows:

S08EL includes the SLIC peripheral, which supports LIN 2.0 and SAE J2602 protocols. It also features 16 interrupt pins and up to 512 bytes of EEPROM.

S08SH features the MTIM peripheral, has only 8 interrupt pins, and supports a ganged output option that allows a single write to change the state of multiple pins simultaneously.

S08SG is similar to the S08SH in terms of pinout, tools, and software compatibility. However, it offers a wider range of package options.

Best regards,
Pablo