MC9S08SH obsolete info

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S08SH obsolete info

跳至解决方案
2,592 次查看
anandhram1988
Contributor I

hi, anybody can inform please the direct replacement for MC9S08SH32 ?

 

i found below, MC9S08SG32 and MC9S08EL32

in this case i would like to know the main differences between 

MC9S08SH32 vs  MC9S08SG32  vs MC9S08EL32

Many thanks in advance

1 解答
2,539 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @anandhram1988,

The differences between the S08SH, S08SG, and S08EL are as follows:

S08EL includes the SLIC peripheral, which supports LIN 2.0 and SAE J2602 protocols. It also features 16 interrupt pins and up to 512 bytes of EEPROM.

S08SH features the MTIM peripheral, has only 8 interrupt pins, and supports a ganged output option that allows a single write to change the state of multiple pins simultaneously.

S08SG is similar to the S08SH in terms of pinout, tools, and software compatibility. However, it offers a wider range of package options.

Best regards,
Pablo

在原帖中查看解决方案

1 回复
2,540 次查看
Pablo_Ramos
NXP Employee
NXP Employee

Hi @anandhram1988,

The differences between the S08SH, S08SG, and S08EL are as follows:

S08EL includes the SLIC peripheral, which supports LIN 2.0 and SAE J2602 protocols. It also features 16 interrupt pins and up to 512 bytes of EEPROM.

S08SH features the MTIM peripheral, has only 8 interrupt pins, and supports a ganged output option that allows a single write to change the state of multiple pins simultaneously.

S08SG is similar to the S08SH in terms of pinout, tools, and software compatibility. However, it offers a wider range of package options.

Best regards,
Pablo