MC9S08QG  Freescale-provided equate file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MC9S08QG  Freescale-provided equate file

跳至解决方案
975 次查看
PKnail
Contributor I

The MC9S08QG8 and MC9S08QG8 data book shows all the address assignments in tables 4-1, 4-2, 4-3 and 4-4.

 

The book says that the names are "used in the Freescale Semiconductor-provided equate file for the MC9S08QG4/8."

 

Where do they have those files?

 

TIA.

标签 (1)
0 项奖励
回复
1 解答
853 次查看
peg
Senior Contributor IV

Hello and welcome to the fora,

 

I believe the only place these are available is included with Codewarrior.

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
854 次查看
peg
Senior Contributor IV

Hello and welcome to the fora,

 

I believe the only place these are available is included with Codewarrior.

 

0 项奖励
回复