MC9S08QG  Freescale-provided equate file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08QG  Freescale-provided equate file

Jump to solution
971 Views
PKnail
Contributor I

The MC9S08QG8 and MC9S08QG8 data book shows all the address assignments in tables 4-1, 4-2, 4-3 and 4-4.

 

The book says that the names are "used in the Freescale Semiconductor-provided equate file for the MC9S08QG4/8."

 

Where do they have those files?

 

TIA.

Labels (1)
0 Kudos
Reply
1 Solution
849 Views
peg
Senior Contributor IV

Hello and welcome to the fora,

 

I believe the only place these are available is included with Codewarrior.

 

View solution in original post

0 Kudos
Reply
1 Reply
850 Views
peg
Senior Contributor IV

Hello and welcome to the fora,

 

I believe the only place these are available is included with Codewarrior.

 

0 Kudos
Reply