MC9S08QG  Freescale-provided equate file

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08QG  Freescale-provided equate file

ソリューションへジャンプ
1,616件の閲覧回数
PKnail
Contributor I

The MC9S08QG8 and MC9S08QG8 data book shows all the address assignments in tables 4-1, 4-2, 4-3 and 4-4.

 

The book says that the names are "used in the Freescale Semiconductor-provided equate file for the MC9S08QG4/8."

 

Where do they have those files?

 

TIA.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,494件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora,

 

I believe the only place these are available is included with Codewarrior.

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,495件の閲覧回数
peg
Senior Contributor IV

Hello and welcome to the fora,

 

I believe the only place these are available is included with Codewarrior.

 

0 件の賞賛
返信