MC9S08PL16 Bootloader Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08PL16 Bootloader Example

4,097件の閲覧回数
0800200c9a66
Contributor I

Hello,

I am in need of a concrete example showing how to implement the Developer’s Serial Bootloader from AN2295 on an MC9S08PL16.

I have been researching how to implement this, but seem to be plagued with dead links, incomplete download packages, and a general lack of awareness on how this needs to be completed.

I would like to know where to obtain the bootloader slave firmware, and how to configure/install it on the MC9S08PL16 processor. 

I would like to know where to obtain the host application and how to configure/load the s19 file over serial to the slave.

In my specific case, I have written an application with Processor Expert in CW 11.1. I am able to load this application and debug/run on the MC9S08PL16 using a PE Multilink Universal. My application makes use of the watchdog timer, SCI0, MTIM0, and a few GPIO. Now, I would like to add the bootloader to be able to load new application firmware over serial.

Please let me know if you have experience bootloading this uC.

Thanks.

タグ(2)
0 件の賞賛
返信
4 返答(返信)

3,839件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi I found this old sample, this is for the s08pt60 but it can help you, please check it 

Regards

0 件の賞賛
返信

3,839件の閲覧回数
jonathanmcclain
Contributor I

Hello Vicente.

Would you happen to have a similarly updated AN2295 project for the DZ60, which would work on CW 10.7 and above? 

I have the project software for AN2295SW, but the settings for the S08DZ are all old *.mcp projects, and Codewarrior 10.7 will not import it correctly.  I have been trying to rebuild that project for the DZ60 in CW 10.7 with no luck.    

It seems that any work with AN2295 software ended around 2012.  Is there an updated AN2295SW project zip that is compatible with CW 10.7 or higher?

Thanks much,

Jon

0 件の賞賛
返信

3,839件の閲覧回数
tonyp
Senior Contributor II

If it doesn't have to be this specific one, there is a different DZ60 bootloader available here: GitHub

0 件の賞賛
返信

3,839件の閲覧回数
0800200c9a66
Contributor I

I modified this code and it works now. Thanks.

0 件の賞賛
返信