MC9S08DZ128CLH replacement part

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC9S08DZ128CLH replacement part

Jump to solution
2,025 Views
nxf59945
NXP Employee
NXP Employee

Dear Sir:

Due to MC9S08DZ128CLH part shortage issue, my customer would like to survey if S9S08DZ128F2CLH could be replacement part without need to modify layout and firmware code, needs your comments to confirm, thanks!

B.R.

Eric

0 Kudos
Reply
1 Solution
2,011 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

your customer need to check if the errata for the mask set 2M78G (mask set for the auto part) are not affecting the part that normally used 

 

the pinout is the same and if the errata does not affect the customer program then, yes it is the same 

 

I hope this will help you

 

Regards

 

View solution in original post

0 Kudos
Reply
2 Replies
2,012 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

your customer need to check if the errata for the mask set 2M78G (mask set for the auto part) are not affecting the part that normally used 

 

the pinout is the same and if the errata does not affect the customer program then, yes it is the same 

 

I hope this will help you

 

Regards

 

0 Kudos
Reply
2,007 Views
nxf59945
NXP Employee
NXP Employee

Thanks Vicente's comments and instant help!

B.R.

Eric

0 Kudos
Reply