MC9S08DZ128CLH replacement part

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC9S08DZ128CLH replacement part

ソリューションへジャンプ
2,126件の閲覧回数
nxf59945
NXP Employee
NXP Employee

Dear Sir:

Due to MC9S08DZ128CLH part shortage issue, my customer would like to survey if S9S08DZ128F2CLH could be replacement part without need to modify layout and firmware code, needs your comments to confirm, thanks!

B.R.

Eric

0 件の賞賛
返信
1 解決策
2,112件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

your customer need to check if the errata for the mask set 2M78G (mask set for the auto part) are not affecting the part that normally used 

 

the pinout is the same and if the errata does not affect the customer program then, yes it is the same 

 

I hope this will help you

 

Regards

 

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,113件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi

 

your customer need to check if the errata for the mask set 2M78G (mask set for the auto part) are not affecting the part that normally used 

 

the pinout is the same and if the errata does not affect the customer program then, yes it is the same 

 

I hope this will help you

 

Regards

 

0 件の賞賛
返信
2,108件の閲覧回数
nxf59945
NXP Employee
NXP Employee

Thanks Vicente's comments and instant help!

B.R.

Eric

0 件の賞賛
返信